Other Parts Discussed in Thread: MSP-EXP430FR5994
Tool/software: Code Composer Studio
Hello,
Compiling any CTPL project in CCS 10 throws symbols undefined error in ctpl_msp430fr5994.c file. See attached image at the end for the list of symbols undefined.
I checked the msp430fr5994.h file in my CCS install dir . These port names are undefined. Only PORTA, PORTJ and PORT1 is defined in the header file.
I followed the instruction to import an example project from FRAM utilities and also to create an empty CTPL project. The same error persists. How should I proceed?
There is also an error in ctpl_low_level.asm. Not sure exactly where the error is because it does not show up the error description.
Thanks,
Archies