Part Number: MSP-EXP430G2ET
Other Parts Discussed in Thread: BOOST-DRV8711, DRV8711, MSP-EXP430F5529LP
Hi, I got a MSP-EXP430E2GT board and boost-drv8711 to test stepper motors.(Not MSP-EXP430G2 board)
I load the firmware to the MCU, close the CCS,and than run the GUI with runtime 6.2.0.0.
However, the GUI can't recognize the firmware verion, full scale current. And with Register Tab, I call Read ALL command,there is no feedback.
Seems there is no SPI communication,also no action on the bus throuth the scope.
I can measure the UART activity from the bus of MSP430, both tx and rx, with a 5ms message periodly.
I already put the rx and tx pin horizontally on the launchpad, and remove the J6 and J7 to enable the SPI port.Also the VM of boost-drv8711 is 12V, with no motor connected now.
Any suggestion for me to check the issue?

Regards
Arrow