This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to port the Compute through power loss FRAM utility using the GNU v8.3.0.16 compiler for the MSP430FR5994.
Through this thread I came to know that The two components that would need to be ported from the TI compiler to GCC are the the linker files (placing all RAM data into FRAM with the exception of the stack) and the low-level assembly routine. I have updated the low level assembly file and with the default linker for the 5994,
I was able to compile the example code from the resource explorer(The internal ADC monitoring for checkpointing) but the code doesn't seem to work. The GPIO toggling is itself indifferent.
Through this thread , I was able to recolonize the issues and tried to modify the linker files(wrt the 5994 device) and even for the watchdog timer issue, but for some reason it just doesn't compile with the updated linker file. (I did this comparing the linker file from the example code , which compiles with the TI compiler)
I have attached the project here ctpl_with_gcc_debug.zip - which is with the default linker.
The updated linker file which doesn't compile is this
/* ============================================================================ */ /* Copyright (c) 2015, Texas Instruments Incorporated */ /* All rights reserved. */ /* */ /* Redistribution and use in source and binary forms, with or without */ /* modification, are permitted provided that the following conditions */ /* are met: */ /* */ /* * Redistributions of source code must retain the above copyright */ /* notice, this list of conditions and the following disclaimer. */ /* */ /* * Redistributions in binary form must reproduce the above copyright */ /* notice, this list of conditions and the following disclaimer in the */ /* documentation and/or other materials provided with the distribution. */ /* */ /* * Neither the name of Texas Instruments Incorporated nor the names of */ /* its contributors may be used to endorse or promote products derived */ /* from this software without specific prior written permission. */ /* */ /* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */ /* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, */ /* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR */ /* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR */ /* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, */ /* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, */ /* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */ /* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, */ /* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR */ /* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, */ /* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* ============================================================================ */ /* This file supports MSP430FR5994 devices. */ /* Default linker script, for normal executables */ /* 1.207 */ OUTPUT_ARCH(msp430) ENTRY(_start) MEMORY { TINYRAM : ORIGIN = 0xA, LENGTH = 0x0016 BSL : ORIGIN = 0x1000, LENGTH = 0x0800 RAM : ORIGIN = 0x1C00, LENGTH = 0x1000 LEARAM : ORIGIN = 0x2C00, LENGTH = 0x0EC8 LEASTACK : ORIGIN = 0x3AC8, LENGTH = 0x0138 INFOMEM : ORIGIN = 0x1800, LENGTH = 0x0200 INFOD : ORIGIN = 0x1800, LENGTH = 0x0080 INFOC : ORIGIN = 0x1880, LENGTH = 0x0080 INFOB : ORIGIN = 0x1900, LENGTH = 0x0080 INFOA : ORIGIN = 0x1980, LENGTH = 0x0080 FRAM : ORIGIN = 0x4000, LENGTH = 0xBF80 /* END=0xFF7F, size 49024 */ FRAM2 : ORIGIN = 0x10000, LENGTH = 0x34000 HIFRAM (rxw) : ORIGIN = 0x00010000, LENGTH = 0x00033FFF JTAGSIGNATURE : ORIGIN = 0xFF80, LENGTH = 0x0004 BSLSIGNATURE : ORIGIN = 0xFF84, LENGTH = 0x0004 IPESIGNATURE : ORIGIN = 0xFF88, LENGTH = 0x0008 VECT0 : ORIGIN = 0xFF90, LENGTH = 0x0002 VECT1 : ORIGIN = 0xFF92, LENGTH = 0x0002 VECT2 : ORIGIN = 0xFF94, LENGTH = 0x0002 VECT3 : ORIGIN = 0xFF96, LENGTH = 0x0002 VECT4 : ORIGIN = 0xFF98, LENGTH = 0x0002 VECT5 : ORIGIN = 0xFF9A, LENGTH = 0x0002 VECT6 : ORIGIN = 0xFF9C, LENGTH = 0x0002 VECT7 : ORIGIN = 0xFF9E, LENGTH = 0x0002 VECT8 : ORIGIN = 0xFFA0, LENGTH = 0x0002 VECT9 : ORIGIN = 0xFFA2, LENGTH = 0x0002 VECT10 : ORIGIN = 0xFFA4, LENGTH = 0x0002 VECT11 : ORIGIN = 0xFFA6, LENGTH = 0x0002 VECT12 : ORIGIN = 0xFFA8, LENGTH = 0x0002 VECT13 : ORIGIN = 0xFFAA, LENGTH = 0x0002 VECT14 : ORIGIN = 0xFFAC, LENGTH = 0x0002 VECT15 : ORIGIN = 0xFFAE, LENGTH = 0x0002 VECT16 : ORIGIN = 0xFFB0, LENGTH = 0x0002 VECT17 : ORIGIN = 0xFFB2, LENGTH = 0x0002 VECT18 : ORIGIN = 0xFFB4, LENGTH = 0x0002 VECT19 : ORIGIN = 0xFFB6, LENGTH = 0x0002 VECT20 : ORIGIN = 0xFFB8, LENGTH = 0x0002 VECT21 : ORIGIN = 0xFFBA, LENGTH = 0x0002 VECT22 : ORIGIN = 0xFFBC, LENGTH = 0x0002 VECT23 : ORIGIN = 0xFFBE, LENGTH = 0x0002 VECT24 : ORIGIN = 0xFFC0, LENGTH = 0x0002 VECT25 : ORIGIN = 0xFFC2, LENGTH = 0x0002 VECT26 : ORIGIN = 0xFFC4, LENGTH = 0x0002 VECT27 : ORIGIN = 0xFFC6, LENGTH = 0x0002 VECT28 : ORIGIN = 0xFFC8, LENGTH = 0x0002 VECT29 : ORIGIN = 0xFFCA, LENGTH = 0x0002 VECT30 : ORIGIN = 0xFFCC, LENGTH = 0x0002 VECT31 : ORIGIN = 0xFFCE, LENGTH = 0x0002 VECT32 : ORIGIN = 0xFFD0, LENGTH = 0x0002 VECT33 : ORIGIN = 0xFFD2, LENGTH = 0x0002 VECT34 : ORIGIN = 0xFFD4, LENGTH = 0x0002 VECT35 : ORIGIN = 0xFFD6, LENGTH = 0x0002 VECT36 : ORIGIN = 0xFFD8, LENGTH = 0x0002 VECT37 : ORIGIN = 0xFFDA, LENGTH = 0x0002 VECT38 : ORIGIN = 0xFFDC, LENGTH = 0x0002 VECT39 : ORIGIN = 0xFFDE, LENGTH = 0x0002 VECT40 : ORIGIN = 0xFFE0, LENGTH = 0x0002 VECT41 : ORIGIN = 0xFFE2, LENGTH = 0x0002 VECT42 : ORIGIN = 0xFFE4, LENGTH = 0x0002 VECT43 : ORIGIN = 0xFFE6, LENGTH = 0x0002 VECT44 : ORIGIN = 0xFFE8, LENGTH = 0x0002 VECT45 : ORIGIN = 0xFFEA, LENGTH = 0x0002 VECT46 : ORIGIN = 0xFFEC, LENGTH = 0x0002 VECT47 : ORIGIN = 0xFFEE, LENGTH = 0x0002 VECT48 : ORIGIN = 0xFFF0, LENGTH = 0x0002 VECT49 : ORIGIN = 0xFFF2, LENGTH = 0x0002 VECT50 : ORIGIN = 0xFFF4, LENGTH = 0x0002 VECT51 : ORIGIN = 0xFFF6, LENGTH = 0x0002 VECT52 : ORIGIN = 0xFFF8, LENGTH = 0x0002 VECT53 : ORIGIN = 0xFFFA, LENGTH = 0x0002 VECT54 : ORIGIN = 0xFFFC, LENGTH = 0x0002 RESETVEC : ORIGIN = 0xFFFE, LENGTH = 0x0002 } SECTIONS { .leaRAM : {} > LEARAM .jtagsignature : {} > JTAGSIGNATURE .bslsignature : {} > BSLSIGNATURE .ipe : { KEEP (*(.ipesignature)) KEEP (*(.jtagpassword)) } > IPESIGNATURE __interrupt_vector_0 : { KEEP (*(__interrupt_vector_0 )) } > VECT0 __interrupt_vector_1 : { KEEP (*(__interrupt_vector_1 )) } > VECT1 __interrupt_vector_2 : { KEEP (*(__interrupt_vector_2 )) } > VECT2 __interrupt_vector_3 : { KEEP (*(__interrupt_vector_3 )) } > VECT3 __interrupt_vector_4 : { KEEP (*(__interrupt_vector_4 )) } > VECT4 __interrupt_vector_5 : { KEEP (*(__interrupt_vector_5 )) } > VECT5 __interrupt_vector_6 : { KEEP (*(__interrupt_vector_6 )) } > VECT6 __interrupt_vector_7 : { KEEP (*(__interrupt_vector_7 )) } > VECT7 __interrupt_vector_8 : { KEEP (*(__interrupt_vector_8 )) } > VECT8 __interrupt_vector_9 : { KEEP (*(__interrupt_vector_9 )) } > VECT9 __interrupt_vector_10 : { KEEP (*(__interrupt_vector_10 )) } > VECT10 __interrupt_vector_11 : { KEEP (*(__interrupt_vector_11 )) } > VECT11 __interrupt_vector_12 : { KEEP (*(__interrupt_vector_12 )) } > VECT12 __interrupt_vector_13 : { KEEP (*(__interrupt_vector_13 )) } > VECT13 __interrupt_vector_14 : { KEEP (*(__interrupt_vector_14 )) } > VECT14 __interrupt_vector_15 : { KEEP (*(__interrupt_vector_15 )) } > VECT15 __interrupt_vector_16 : { KEEP (*(__interrupt_vector_16 )) } > VECT16 __interrupt_vector_17 : { KEEP (*(__interrupt_vector_17 )) } > VECT17 __interrupt_vector_18 : { KEEP (*(__interrupt_vector_18)) KEEP (*(__interrupt_vector_lea)) } > VECT18 __interrupt_vector_19 : { KEEP (*(__interrupt_vector_19)) KEEP (*(__interrupt_vector_port8)) } > VECT19 __interrupt_vector_20 : { KEEP (*(__interrupt_vector_20)) KEEP (*(__interrupt_vector_port7)) } > VECT20 __interrupt_vector_21 : { KEEP (*(__interrupt_vector_21)) KEEP (*(__interrupt_vector_eusci_b3)) } > VECT21 __interrupt_vector_22 : { KEEP (*(__interrupt_vector_22)) KEEP (*(__interrupt_vector_eusci_b2)) } > VECT22 __interrupt_vector_23 : { KEEP (*(__interrupt_vector_23)) KEEP (*(__interrupt_vector_eusci_b1)) } > VECT23 __interrupt_vector_24 : { KEEP (*(__interrupt_vector_24)) KEEP (*(__interrupt_vector_eusci_a3)) } > VECT24 __interrupt_vector_25 : { KEEP (*(__interrupt_vector_25)) KEEP (*(__interrupt_vector_eusci_a2)) } > VECT25 __interrupt_vector_26 : { KEEP (*(__interrupt_vector_26)) KEEP (*(__interrupt_vector_port6)) } > VECT26 __interrupt_vector_27 : { KEEP (*(__interrupt_vector_27)) KEEP (*(__interrupt_vector_port5)) } > VECT27 __interrupt_vector_28 : { KEEP (*(__interrupt_vector_28)) KEEP (*(__interrupt_vector_timer4_a1)) } > VECT28 __interrupt_vector_29 : { KEEP (*(__interrupt_vector_29)) KEEP (*(__interrupt_vector_timer4_a0)) } > VECT29 __interrupt_vector_30 : { KEEP (*(__interrupt_vector_30)) KEEP (*(__interrupt_vector_aes256)) } > VECT30 __interrupt_vector_31 : { KEEP (*(__interrupt_vector_31)) KEEP (*(__interrupt_vector_rtc_c)) } > VECT31 __interrupt_vector_32 : { KEEP (*(__interrupt_vector_32)) KEEP (*(__interrupt_vector_port4)) } > VECT32 __interrupt_vector_33 : { KEEP (*(__interrupt_vector_33)) KEEP (*(__interrupt_vector_port3)) } > VECT33 __interrupt_vector_34 : { KEEP (*(__interrupt_vector_34)) KEEP (*(__interrupt_vector_timer3_a1)) } > VECT34 __interrupt_vector_35 : { KEEP (*(__interrupt_vector_35)) KEEP (*(__interrupt_vector_timer3_a0)) } > VECT35 __interrupt_vector_36 : { KEEP (*(__interrupt_vector_36)) KEEP (*(__interrupt_vector_port2)) } > VECT36 __interrupt_vector_37 : { KEEP (*(__interrupt_vector_37)) KEEP (*(__interrupt_vector_timer2_a1)) } > VECT37 __interrupt_vector_38 : { KEEP (*(__interrupt_vector_38)) KEEP (*(__interrupt_vector_timer2_a0)) } > VECT38 __interrupt_vector_39 : { KEEP (*(__interrupt_vector_39)) KEEP (*(__interrupt_vector_port1)) } > VECT39 __interrupt_vector_40 : { KEEP (*(__interrupt_vector_40)) KEEP (*(__interrupt_vector_timer1_a1)) } > VECT40 __interrupt_vector_41 : { KEEP (*(__interrupt_vector_41)) KEEP (*(__interrupt_vector_timer1_a0)) } > VECT41 __interrupt_vector_42 : { KEEP (*(__interrupt_vector_42)) KEEP (*(__interrupt_vector_dma)) } > VECT42 __interrupt_vector_43 : { KEEP (*(__interrupt_vector_43)) KEEP (*(__interrupt_vector_eusci_a1)) } > VECT43 __interrupt_vector_44 : { KEEP (*(__interrupt_vector_44)) KEEP (*(__interrupt_vector_timer0_a1)) } > VECT44 __interrupt_vector_45 : { KEEP (*(__interrupt_vector_45)) KEEP (*(__interrupt_vector_timer0_a0)) } > VECT45 __interrupt_vector_46 : { KEEP (*(__interrupt_vector_46)) KEEP (*(__interrupt_vector_adc12_b)) } > VECT46 __interrupt_vector_47 : { KEEP (*(__interrupt_vector_47)) KEEP (*(__interrupt_vector_eusci_b0)) } > VECT47 __interrupt_vector_48 : { KEEP (*(__interrupt_vector_48)) KEEP (*(__interrupt_vector_eusci_a0)) } > VECT48 __interrupt_vector_49 : { KEEP (*(__interrupt_vector_49)) KEEP (*(__interrupt_vector_wdt)) } > VECT49 __interrupt_vector_50 : { KEEP (*(__interrupt_vector_50)) KEEP (*(__interrupt_vector_timer0_b1)) } > VECT50 __interrupt_vector_51 : { KEEP (*(__interrupt_vector_51)) KEEP (*(__interrupt_vector_timer0_b0)) } > VECT51 __interrupt_vector_52 : { KEEP (*(__interrupt_vector_52)) KEEP (*(__interrupt_vector_comp_e)) } > VECT52 __interrupt_vector_53 : { KEEP (*(__interrupt_vector_53)) KEEP (*(__interrupt_vector_unmi)) } > VECT53 __interrupt_vector_54 : { KEEP (*(__interrupt_vector_54)) KEEP (*(__interrupt_vector_sysnmi)) } > VECT54 __reset_vector : { KEEP (*(__interrupt_vector_55)) KEEP (*(__interrupt_vector_reset)) KEEP (*(.resetvec)) } > RESETVEC .lower.rodata : { . = ALIGN(2); *(.lower.rodata.* .lower.rodata) } > ROM .rodata : { . = ALIGN(2); *(.plt) *(.rodata .rodata.* .gnu.linkonce.r.* .const .const:*) *(.rodata1) *(.lower.rodata.* .lower.rodata) /* Note: By default we do not have this line: *(.either.rodata.*) *(.either.rodata) defined here, or anywhere else in this script. This is deliberate. The algorithm in the linker that automatically places rodata into either the .rodata or the .upper.rodata sections relies upon the fact that the .either.rodata section is not defined, and that the .upper.rodata section is defined. If the .upper.rodata is not defined in this script then the line above should be restored so that code compiled with -mdata-region=either enabled will still work. The same reasoning applies to the absence of definitions for the .either.text, .either.data and .either.bss sections as well. */ *(.eh_frame_hdr) KEEP (*(.eh_frame)) KEEP (*(.gcc_except_table)) *(.gcc_except_table.*) PROVIDE (__preinit_array_start = .); KEEP (*(.preinit_array)) PROVIDE (__preinit_array_end = .); PROVIDE (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array)) PROVIDE (__init_array_end = .); PROVIDE (__fini_array_start = .); KEEP (*(.fini_array)) KEEP (*(SORT(.fini_array.*))) PROVIDE (__fini_array_end = .); /* Note: Separate .rodata section for sections which are read only but which older linkers treat as read-write. This prevents older linkers from marking the entire .rodata section as read-write. */ /*.rodata2 : { . = ALIGN(2); *(.eh_frame_hdr) KEEP (*(.eh_frame))*/ /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin*.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE (*crtend*.o ) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) KEEP (*crtbegin*.o(.dtors)) KEEP (*(EXCLUDE_FILE (*crtend*.o ) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) } > ROM /* This section contains data that is not initialised during load or application reset. */ /*.persistent : { . = ALIGN(2); PROVIDE (__persistent_start = .); *(.persistent) . = ALIGN(2); PROVIDE (__persistent_end = .); } > ROM */ .upper.rodata : { /* Note: If this section is not defined then please add: *(.either.rodata.*) *(.either.rodata) to the definition of the .rodata section above. This will allow code compiled with -mdata-region=either to work properly. */ *(.upper.rodata.* .upper.rodata) } > HIFRAM .tinyram : {} > TINYRAM .lower.data : { . = ALIGN(2); PROVIDE (__datastart = .); *(.lower.data.* .lower.data) } > RAM AT> ROM .data : { . = ALIGN(2); PROVIDE (__datastart = .); KEEP (*(.jcr)) *(.data.rel.ro.local) *(.data.rel.ro*) *(.dynamic) *(.data .data.* .gnu.linkonce.d.*) KEEP (*(.gnu.linkonce.d.*personality*)) SORT(CONSTRUCTORS) *(.data1) *(.got.plt) *(.got) /* We want the small data sections together, so single-instruction offsets can access them all, and initialized data all before uninitialized, so we can shorten the on-disk segment size. */ . = ALIGN(2); *(.sdata .sdata.* .gnu.linkonce.s.* D_2 D_1) /* See the note in .rodata section about why we do not have this line here: *(.either.data.* .either.data) */ . = ALIGN(2); *(.lower.data.* .lower.data) . = ALIGN(2); _edata = .; PROVIDE (edata = .); PROVIDE (__dataend = .); } > RAM AT> ROM /* Note that crt0 assumes this is a multiple of two; all the start/stop symbols are also assumed word-aligned. */ PROVIDE(__romdatastart = LOADADDR(.data)); PROVIDE (__romdatacopysize = SIZEOF(.data)); .upper.data : { __upper_data_init = LOADADDR (.upper.data); /* Status word. */ SHORT(1); __high_datastart = .; *(.upper.data.* .upper.data) __high_dataend = .; } > HIFRAM AT> ROM __rom_highdatacopysize = SIZEOF(.upper.data) - 2; __rom_highdatastart = LOADADDR(.upper.data) + 2; .lower.bss : { . = ALIGN(2); PROVIDE (__bssstart = .); *(.lower.bss.* .lower.bss) } > RAM .bss : { . = ALIGN(2); PROVIDE (__bssstart = .); *(.dynbss) *(.sbss .sbss.*) *(.bss .bss.* .gnu.linkonce.b.*) *(.lower.bss.* .lower.bss) /* See the note in .rodata section about why we do not have this line here: *(.either.bss.* .either.bss) */ . = ALIGN(2); *(COMMON) PROVIDE (__bssend = .); } > RAM PROVIDE (__bsssize = SIZEOF(.lower.bss) + SIZEOF(.bss)); /* This section contains data that is not initialised during load or application reset. */ .noinit (NOLOAD) : { . = ALIGN(2); PROVIDE (__noinit_start = .); *(.noinit) . = ALIGN(2); PROVIDE (__noinit_end = .); } > RAM .upper.bss : { /* Note - if this section is not going to be defined then please add this line back into the definition of the .bss section above: *(.either.bss.* .either.bss) */ . = ALIGN(2); __high_bssstart = .; *(.upper.bss.* .upper.bss) . = ALIGN(2); __high_bssend = .; } > HIFRAM __high_bsssize = SIZEOF(.upper.bss); .ctpl (ORIGIN (FRAM)): { . = ALIGN(2); PROVIDE (__ctpl = .); *(.ctpl) . = ALIGN(2); PROVIDE (__ctpl_end = .); } > FRAM = 0x0 /* We create this section so that "end" will always be in the RAM region (matching .stack below), even if the .bss section is empty. */ /* .heap (NOLOAD) : { . = ALIGN(2); __heap_start__ = .; _end = __heap_start__; PROVIDE (end = .); KEEP (*(.heap)) _end = .; PROVIDE (end = .); /* This word is here so that the section is not empty, and thus not discarded by the linker. The actual value does not matter and is ignored. */ /* LONG(0); __heap_end__ = .; __HeapLimit = __heap_end__; } > RAM */ /* WARNING: Do not place anything in RAM here. The heap section must be the last section in RAM and the stack section must be placed at the very end of the RAM region. */ .stack (ORIGIN (RAM) + LENGTH(RAM)) : { PROVIDE (__stack = .); *(.stack) } .lower.text : { . = ALIGN(2); *(.lower.text.* .lower.text) } > ROM .text : { PROVIDE (_start = .); . = ALIGN(2); KEEP (*(SORT(.crt_*))) . = ALIGN(2); KEEP (*(.lowtext)) . = ALIGN(2); *(.lower.text.* .lower.text) . = ALIGN(2); *(.text .stub .text.* .gnu.linkonce.t.* .text:*) /* See the note in .rodata section about why we do not have this line here: *(.either.text.* .either.text) */ KEEP (*(.text.*personality*)) /* .gnu.warning sections are handled specially by elf32.em. */ *(.gnu.warning) *(.interp .hash .dynsym .dynstr .gnu.version*) PROVIDE (__etext = .); PROVIDE (_etext = .); PROVIDE (etext = .); . = ALIGN(2); KEEP (*(.init)) KEEP (*(.fini)) KEEP (*(.tm_clone_table)) } > ROM .upper.text : { /* Note - if this section is not going to be included in the script then please add this line back into the definition of the .text section above: *(.either.text.* .either.text) */ . = ALIGN(2); *(.upper.text.* .upper.text) } > HIFRAM /* MSP430 INFO FLASH MEMORY SEGMENTS */ .infoD : {} > INFOD .infoC : {} > INFOC .infoB : {} > INFOB .infoA : {} > INFOA /* The rest are all not normally part of the runtime image. */ .MSP430.attributes 0 : { KEEP (*(.MSP430.attributes)) KEEP (*(.gnu.attributes)) KEEP (*(__TI_build_attributes)) } /* Stabs debugging sections. */ .stab 0 : { *(.stab) } .stabstr 0 : { *(.stabstr) } .stab.excl 0 : { *(.stab.excl) } .stab.exclstr 0 : { *(.stab.exclstr) } .stab.index 0 : { *(.stab.index) } .stab.indexstr 0 : { *(.stab.indexstr) } .comment 0 : { *(.comment) } /* DWARF debug sections. Symbols in the DWARF debugging sections are relative to the beginning of the section so we begin them at 0. */ /* DWARF 1. */ .debug 0 : { *(.debug) } .line 0 : { *(.line) } /* GNU DWARF 1 extensions. */ .debug_srcinfo 0 : { *(.debug_srcinfo) } .debug_sfnames 0 : { *(.debug_sfnames) } /* DWARF 1.1 and DWARF 2. */ .debug_aranges 0 : { *(.debug_aranges) } .debug_pubnames 0 : { *(.debug_pubnames) } /* DWARF 2. */ .debug_info 0 : { *(.debug_info .gnu.linkonce.wi.*) } .debug_abbrev 0 : { *(.debug_abbrev) } .debug_line 0 : { *(.debug_line .debug_line.* .debug_line_end ) } .debug_frame 0 : { *(.debug_frame) } .debug_str 0 : { *(.debug_str) } .debug_loc 0 : { *(.debug_loc) } .debug_macinfo 0 : { *(.debug_macinfo) } /* SGI/MIPS DWARF 2 extensions. */ .debug_weaknames 0 : { *(.debug_weaknames) } .debug_funcnames 0 : { *(.debug_funcnames) } .debug_typenames 0 : { *(.debug_typenames) } .debug_varnames 0 : { *(.debug_varnames) } /* DWARF 3 */ .debug_pubtypes 0 : { *(.debug_pubtypes) } .debug_ranges 0 : { *(.debug_ranges) } /* DWARF Extension. */ .debug_macro 0 : { *(.debug_macro) } /DISCARD/ : { *(.note.GNU-stack) } } /****************************************************************************/ /* Include peripherals memory map */ /****************************************************************************/ INCLUDE msp430fr5994_symbols.ld
Any help would be greatly appreciated.
Hello,
The MSP430 GCC Toolchain User’s Guide should be a good resource for this exercise.
Thanks for the reply James. I have been able to successfully compile the low level assembly file but could you please give me an insight of the specific changes that has to be done on the linker file, in order to successfully port the ctpl on to work with the GCC. sorry I am a bit new to the linker scripts.
Your modified linker script references the symbol "ROM" which isn't defined. (Typically used on flash parts.) The original version uses "FRAM".
Expanding on that a bit, here is part of the script:
.lower.data : { . = ALIGN(2); PROVIDE (__datastart = .); *(.lower.data.* .lower.data) } > RAM AT> FRAM
The reason for this is that while the variables live in RAM their initial values are stored in FRAM. The startup routines copy the initial values.
It would appear that what you need is ">FRAM AT> FRAM". Kind of redundant and it wastes space but disabling the copy of initial values would require a dive into the startup code. The manual (slau646) describes how to insert functions into the initialization sequence to disable the watchdog but doesn't say anything about replacing or disabling existing routines.
You probably also want to change the bss from RAM to FRAM since uninitialized variables live there.
Thanks a lot David, let me try your suggestion and see it out. so would you suggest me using the default linker file that you get with a gcc project and modifying it to have >FRAM AT> FRAM disabling the copy of initial values and change the bss from RAM to FRAM
And I guess the Heap should be placed on the FRAM and the stack should remain in the RAM? Like in the code snippet below. Also should I split the FRAM into two spaces(for read and write) and how can this be linked with the ctpl library then?
.heap (NOLOAD) : { . = ALIGN(2); __heap_start__ = .; _end = __heap_start__; PROVIDE (end = .); KEEP (*(.heap)) _end = .; PROVIDE (end = .); /* This word is here so that the section is not empty, and thus not discarded by the linker. The actual value does not matter and is ignored. */ LONG(0); __heap_end__ = .; __HeapLimit = __heap_end__; } > ROM /* WARNING: Do not place anything in RAM here. The heap section must be the last section in RAM and the stack section must be placed at the very end of the RAM region. */ .stack (ORIGIN (RAM) + LENGTH(RAM)) : { PROVIDE (__stack = .); *(.stack) } .lower.text : { . = ALIGN(2); *(.lower.text.* .lower.text) } > RAM
At the same time I am using the below code snippet in the low level assembly file but the compiler always gives me an error saying ../fram-utilities/ctpl/ctpl_low_level.s:126: Error: extra characters '(((0x0080)+(0x0040)+(0x0020)+(0x0010)))' at end of immediate expression '#__bis_SR_register(((0x0080)+(0x0040)+(0x0020)+(0x0010)))'.
ctpl_enterLpm: benchmark ; Toggle the CTPL benchmark pin lpmDebug ; Optional LPMx.5 debug mode* mov.b #PMMPW_H,&PMMCTL0_H ; Set LPMx.5 bit mov.b #PMMREGOFF,&PMMCTL0_L ; Set LPMx.5 bit bis.w #LPM4, SR /*# Enter LPMx.5 mode*/ nop
Could anyone help me with this as well as to why that happens?
Did you define __STDC__ somewhere in that assembly language file? The 5994.h file uses that symbol to select between definitions of LPM4 suitable for the assembler or C. You got the C version.
I have attached my overall implementation here ctpl_with_gcc.zip. Could you just help me debug this and see if I am completely doing it wrong?
It was defined somewhere. If you can't track down where, then you could use the C version for LPM4 which is LPM4_bits.
**Attention** This is a public forum