Part Number: MSP430F5249
Other Parts Discussed in Thread: MSP430F5529
How many pwm signals can be generated using TIMER_A(MSP430F5249)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5249
Other Parts Discussed in Thread: MSP430F5529
How many pwm signals can be generated using TIMER_A(MSP430F5249)?
Part Number: MSP430F5249
How to update duty cycle runtime?
while generation of PWM whether is it requires to start and stop pwm?
Please share if any reference for the above.
using driver library for implementation
//!
//!Tested On: MSP430F5529
//! -------------------
//! /|\| |
//! | | |
//! --|RST |
//! | |
//! | P2.0/TA1.1|--> CCR1 - 75% PWM
//! | P2.1/TA1.2|--> CCR2 - 25% PWM
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - Timer peripheral
//! - GPIO Port peripheral
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - NONE
//!
//
//*****************************************************************************
#include "driverlib.h"
#define TIMER_PERIOD 127
#define DUTY_CYCLE1 32
#define DUTY_CYCLE2 96
Hello,
For future posts, please use a thread title that's more descriptive than just the part number of your device - summarize the issue or question. This will help others in our community find your threads more easily, especially if they have the same question. I've updated the title of this thread already.
How many pwm signals can be generated using TIMER_A(MSP430F5249)?
You can find out how many PWM signals can be generated from each Timer module by referring to Table 6-1. Device Comparison in the datasheet. See footnote (3) to understand how to interpret the numbers (e.g. 5, 3, 3). Basically, each number represents the number of possible PWM outputs per Timer instantiation.
How to update duty cycle runtime?
while generation of PWM whether is it requires to start and stop pwm?
Please share if any reference for the above.
using driver library for implementation
I think Leo already explained this in the following thread.
**Attention** This is a public forum