Hi ,
I have a rather puzzling issue. I get the following error when trying to debug the MSP-EXP432P401R using the BlinkLED_MSP432P401R example:
CORTEX_M4_0: Error connecting to the target: (Error -1063 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver. (Emulation package 6.0.14.5)
I have been able to run several programs up until earlier this morning, and, all of the sudden, the board just stopped communicating.
Was there a recent update?
I have downloaded and installed (re-installed?) the ti_emupack_setup_6.0.14.5_win_32.exe in an attempt to fix any software driver issues, but the problem remains unchanged.