This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430G2553: MSP430G2553 and LCD interface

Part Number: MSP430G2553

Tool/software: TI C/C++ Compiler

Hi ,

With the reference to this link, i have changed some pin assignments and compiled the program and dumped on to msp430g2553.

On the launchpad MSP-EXP430G2 its working fine,after the reset and able to display on the LCD screen.

but when i am dumping to the stand alone board of the same microcontroller its not working all the connection are fine,but is not displaying on the LCD.

Is anything going wrong ,Should i add any thing more to code to make it work.

/* This program is an example of HD44780 driver no busy check
 Original from Marek Prochazka, adapted and debugged then released to public domain in TI e2e.
 This program use a bit free assignment to lcd pinout so 6 free pin can be connected to LCD any way.
 uP selected from Project setting. Tested on an LCD 16x2 and MSP430G2231
*/

//#include "io430.h"
//<msp430g2452.h>
#include <msp430g2553.h>
// LCD Port assignement
#define LCD_DIR P2DIR
#define LCD_OUT P2OUT

// Lcd Pin assignement
#define LCD_PIN_RS BIT2
//#define LCD_PIN_RW BIT7
#define LCD_PIN_EN BIT3
#define LCD_PIN_D4 BIT6
#define LCD_PIN_D5 BIT7
#define LCD_PIN_D6 BIT4
#define LCD_PIN_D7 BIT5

// Procedure to strobe data to LCD register
void LCDPulseEN(void)
{ // Set Enable active
  __delay_cycles(20);
  LCD_OUT |= LCD_PIN_EN;
  __delay_cycles(20);
  // Release Strobe
  LCD_OUT &= (~LCD_PIN_EN);
}

// this send 4 bit of data
void SendNibble(char data)
{
  // Clear all data bit
  LCD_OUT &= ~(LCD_PIN_D4|LCD_PIN_D5|LCD_PIN_D6|LCD_PIN_D7);
  // Set data bit on port bit
  if(data & 0x01)
    LCD_OUT |= LCD_PIN_D4;
  if(data & 0x02)
    LCD_OUT |= LCD_PIN_D5;
  if(data & 0x04)
    LCD_OUT |= LCD_PIN_D6;
  if(data & 0x08)
    LCD_OUT |= LCD_PIN_D7;
  // Nibble set complete, send to LCD
  LCDPulseEN();
  __delay_cycles(500);
}

// Send a byte of data to LCD register
void SendByte(unsigned char data)
{
  SendNibble((data>>4) & 0x0F);
  SendNibble((data) & 0x0F);
  __delay_cycles(500);
}

// send a byte to command register
void SendInstruction(unsigned char data)
{
  // Set Register to command
  LCD_OUT &= ~LCD_PIN_RS;
  SendByte(data);
  __delay_cycles(80000);
}

// Send a byte of data to LCD register
void LCDputch(unsigned char data)
{
  // Set Register to data
  LCD_OUT |= LCD_PIN_RS;
  SendByte(data);
  __delay_cycles(500);
}



void InitLCD(void)
{
  // clear all bit of LCD control & data Lines
  LCD_OUT &= ~(LCD_PIN_EN|LCD_PIN_RS); //|LCD_PIN_RW);
  // Set LCD pins to output
  LCD_DIR |=(LCD_PIN_EN|LCD_PIN_RS|LCD_PIN_D4|LCD_PIN_D5|LCD_PIN_D6|LCD_PIN_D7); // |LCD_PIN_RW
  // wait Powerup
  __delay_cycles(100000);
  // LCD can be in an unknown state so set to a known state sending 3 times LCD set to 8 bit mode
  SendNibble(3);
  __delay_cycles(16000);  // Wait for init
  SendNibble(3);
  __delay_cycles(400);
  SendNibble(3);
  __delay_cycles(400);
  // now is 8 bit, sending 2 set mode to 4 bit (0x2n)
  SendNibble(2);
  __delay_cycles(800);
  // Now set to mode 4 bit 2 line 5x7 char
  SendInstruction(0x28);
  __delay_cycles(8000);
  // Make cursor visible one line set to 0x0c to invisible cursor
  SendInstruction(0x0e);//c
  __delay_cycles(800);
  // Clear screen
  SendInstruction(0x01);
  __delay_cycles(8000);
  // Increment address mode
  SendInstruction(0x06);
  __delay_cycles(8000);
  // Set write data address to 0
  SendInstruction(0x80);
}

// Set write cursor to Row and Col
void LCDSetPosition(char Row, char Col)
{
  // if row is not 0 add 0x40 (4 line models require adding 0 20 60 40)
  if(Row)
    Col+=0x40;
  SendInstruction(0x80 | Col);
  __delay_cycles(800);
}

// Clear LCD
void LCDClear(void)
{
SendInstruction(0x01);
  __delay_cycles(100000);
}

// Lcd cursor to first row first column
void LCDGoToHome(void)
{
SendInstruction(0x02);
  __delay_cycles(100000);
}

// Shift left mode
void LCDShiftLeft(void)
{
SendInstruction(0x18);
}

// Shift right mode
void LCDShiftRight(void)
{
SendInstruction(0x1C);
}

// Cursor blinking mode
void LCDBlinkCursor(void)
{
SendInstruction(0x0F);
}

// Print a text line to LCD screen
void LCDPrintString(const char * Text)
{
  while (*Text)
    LCDputch(*Text++);
}

/***************************** 8 MHZ clock config *****************************/
void configureClocks_1MHZ(void)
{
#if 0
  // Set system DCO to 8MHz
 // BCSCTL3 |= LFXT1S_2;                      // LFXT1 = VLO
  IFG1 &= ~OFIFG;                           // Clear OSCFault flag
  __bis_SR_register(SCG1 + SCG0);           // Stop DCO
 // BCSCTL2 |= SELM_1 + DIVM_3;               // MCLK = LFXT1/8
  BCSCTL1 = CALBC1_1MHZ;
  DCOCTL = 0;
  DCOCTL = CALBC1_1MHZ;
  FCTL2 = FWKEY + FSSEL0 + FN1;             // MCLK/3 for Flash Timing Generator
  // Set LFXT1 to the VLO @ 12kHz
 // BCSCTL3 |= LFXT1S_2;
#else
    if (CALBC1_1MHZ==0xFF)					// If calibration constant erased
  {											
    while(1);                               // do not load, trap CPU!!	
  } 
  DCOCTL = 0;                               // Select lowest DCOx and MODx settings
  BCSCTL1 = CALBC1_1MHZ;                    // Set range
  DCOCTL = CALDCO_1MHZ;                     // Set DCO step + modulation */

#endif
  
}


void main (void)
{
  char c;
  int i;
  // Stop watchdog timer to prevent time out reset
  WDTCTL = WDTPW + WDTHOLD;
  configureClocks_1MHZ();
  
  P2SEL &= ~(0xC0);
  P2DIR |= 0xC0;  
  
  InitLCD();
  LCDPrintString("Hello world");
  c='0';
  while(1)
  {
    LCDSetPosition(1,10);
    for(i=0;i<100;i++)
      __delay_cycles(1000);
    LCDputch(c);
    c++;
    if(c>'9') c='0';
  }
}

MSP430 and HD44780

**Attention** This is a public forum