Other Parts Discussed in Thread: EVM430-FR6043, , CAPTIVATE-PGMR, EVM430-FR6047
Hi,
The EVM430-FR6043 reference design uses an 8MHz HF crystal.
The MSP430FR6043 can use an HF crystal within a frequency range from 4MHz up to 24MHz.
I wonder why the designer chose 8MHz HF crystal and how does this relate to energy consumption?
Assuming we use a UssGasDemo - MSP430FR6043EVM_USS_Gas_Demo_EVM_v2_0_AFE3v3_02_30_00_01
or UssWaterDemo - MSP430FR6043EVM_USS_Water_Demo_LPM_02_40_00_00
1)
How will the use of different frequencies of the HF crystal oscillator (4, 8, 16, 24 MHz) affect total energy consumption?
2)
Where can I find the crystals characterization for MSP430FR604x similar to this: https://www.ti.com/lit/pdf/swra495
3)
Assuming, I use a 16MHz HF crystal oscillator on my custom board instead of 8MHz on EVM430-FR6043, how can I modify
\ti\msp\UltrasonicWaterFR604x_02_40_00_00\examples\USS_Water_Demo
to work correctly with this higher frequency?
When I use this USS_Water_Demo unchanged, I see the correct number of pulses, but the gap between bursts is more than twice as expected.
Regards
Adam