Part Number: MSP430FR2512
Other Parts Discussed in Thread: MSP430FR2311, ENERGIA
Tool/software: Code Composer Studio
Please, help me figure out why the CCS is giving me the following error:
MSP430: Error connecting to the target: Unknown device
I am currently trying to program a custom made PCB using the MSP430FR2311 Lauchpad as a programmer for the MSP430FR2512. I am simply connecting the SBWTCK to pin 3 and SBWTDIO to pin 4 of the FR2512. Whenever I program the PCB, I use the 3V3 available from the LP. Both devices also share the same ground pin.
I am using a 1nF capacitor connecting the RST pin to ground, and a 100k resistor pulling the same pin up.
The strange part is that I first ran a test on the MCU on the PCB to unsure that all pins are working, so I simply set all pins as output and made them toggle at 8Hz. This first program loaded without a problem, and whwnver I hook up power to my PCB, I can see that all pins are still toggling at 8Hz. However, when I am trying to load the actual firmware that should run on that device, I get the following error from CCS. I did not change anything on the pins.
I wonder if the fuse could be blown, so I tested with a multimeter. I measure an 8Mohm resistance to ground, and whenever I connect the test pin to 3V3, I can measure 70uA going into the pin.
I don't know if the problem is if the fuse, specially considering that the MCU was not in contact with more than 3V.
Do you know what could be the error?