This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have EK-TM4C1294XL board with Tiva TM4C1294. I would like to trigger the ROM based serial loader that is supposed to present on the chip from the factory. Here are the steps.
1. Use LM Flash programmer, switch to ICDI interface, Flash > Erase entire. Power cycle
2. Switch to Serial UART COM8 interface, Program > select bin file blinky.bin, Address offset = 0x00
3. Click program. Error > Failed to establish comm with target.
Please advise how to troubleshoot this problem.
Regards !
OK, not completely sure why, but I tried a second EK-TM4C1294XL and it worked. Then I went back to the first one and tried it again. This time it worked. It might be that the first time I ran into the issue described in advisory SYSCTL#22. (The ROM does not have the updated SysCtlClockFreqSet function.) Make sure you do not disable auto baud support.