Other Parts Discussed in Thread: TM4C129ENCPDT, UNIFLASH, LMFLASHPROGRAMMER
Dear all friends~
After I modified the flash address in tm4c129encpdt.cmd file, I cannot debug my code(XDS100v2), and the error message is CORTEX_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)
how do I solve this issue? Thanks :-))
MEMORY
{
FLASH (RX) : origin = 0x2800, length = 0xFD800
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
SECTIONS
{
.intvecs: > 0x2800
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}