Hi
I am working on a platform based on a TIVA TM4C1233D5PMI. In the application I need the MCU to keep the time (RTC) when the main power (VCC) is "arbitrarily" removed. Basically I just want the RTC to keep running on the battery when power is removed, such that the time can be used when the power comes back.
According to the TIVA datasheet (and this forum) this seems to be very easy to accomplish using the TIVA hibernation module, the RTC and an external battery.
I have created the below schematic for the hibernation module (basically directly from the datasheet):
I have some questions, for which I have not been able to find clear answers (not clear to me atleast):
- When using the RTC in this "Arbitrary Power Removal" mode (as described in the datasheet), how should I connect the wake pin?
- Is it correct that the RTC can be configured to keep running independent of the main power using the above circuit?
- Is it correct that the MCU will boot normally (POR) whenever the main power is connected, using the above circuit? And that the RTC will be available when it has booted?
I really appreciate any help that you can provide.
Thanks.
Best regards
Christian