This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-CGT: Errors in SPRU514V and SPRUHS1C

Part Number: C2000-CGT

Hi TI expert

The forums are erroring out on me, so I gave up...  here are a few typos that I found.

In SPRUHS1C pg 793

The title "QUADF32 RaH, RbH, RcH" is missing the second input RdH, which is for the x-value.  There is even a description of the D-register in the operands section below.

In SPRU514V pg 170

The inputs for the intrinsic operator  "float __atan2puf32( float x, float y );" are swapped in the documentation, it should be: "float __atan2puf32( float y, float x);"  This was tested to be the case with 20.12.0.STS

Best regards,

Thomas