This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sometime later today - or surely early tomorrow - our forum leader will reach 100K points - simply terrific!
Caring, super-responsive, & detailed tech support - so rare these days - and across every phase of his TM4C devices.
Great job Amit - while some question decisions made from the "mount" - your service here has long been outstanding.
Thanks for the great job you do. Know that your efforts are appreciated...
Cordialement,
cb1 (fixed & mobile) & crue
Hi, Silence has to be broken for this very good news and if flea appear here.. I am ready with electric high voltage burner.
Many thanks Amit for all friendly help and conversation too, I am afraid see you are involved in a so huge work but I forever appreciate passion and kind you apply addressing all question also if worst.
I wish the best for our very great and unique friend.
"Bravo" Amit, congratulation for this but I don't see official recognition nor catering for a so unique rare event.
See you.
Roberto
Amit Ashara said:Thank you all for your kind wishes. Just doing my job and learning alongside all of you
Hi Amit, I am proud see finally your work got light but.. I don't see price on buy it now... If iI can vote for your desing I am proud to do so but I never was able to do, if you can guide me through I proudly do.
Amit Ashara said:(doesn't matter even if you are in school... Luis)
I wish Luis out of school asap and me too as retirement I feel to far due to bad government politics. These tools are to be introduced at school instead of Arduino and Hobby community and also instead of prehistoric PIC from Microchip... I feel a bad behaviour from TIVA series, it appear as me like an expensive hobby marketed device and maybe, if production start, get away TIVA from boards, I am afraid of your great work is really appreciated but commercial section of TI I feel, like other designers say, is not supporting correctly production in front of hobby selling of gifted boards.
Amit Ashara said:May I invite you to the following link... This is the first of 3 designs for which I sought opinion...
Amit, I appreciate a lot your work, it is really amazing and well done, I don't appreciate this:
"Fully assembled board (shown above) developed for testing and performance validation only, not available for sale."
it sound really worst, this is a 200US$ board add on not a 10US$ board sell for less than chip value. Anyway for just less more USD Elektronica sell a more more better board complete of ram controllerless better tft display and a capacitive touch.
I don't like this really worst politics and support of just people coming here to scream support for a product where primary goal of it was teaching on school, they never can produce one unit in the future than ask for home job solved also for nothing like the board value they bought.
SO here person asking have one HTML line modified un underundergraduate student is able to do or one c line of code are best served then engineer developing his board. This Amit is not for your great job, is to TI worst policy. I don't see market share of TIVA chips and number are quite static.