Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Dear All,
I am trying to use USB as well as UART boot-loader to update my firmware. As I am done with both individually, for UART based boot-loader I am using BOOT_SERIAL example and for USB based boot-loader I am using USB_STICK_UPDATE along with USB_DEMO example project.
I go through the Boot_Serial example and I believe that instead of using two different project we can use same Boot_serial example for both UART as well as USB based boot-loader. But when I am defining the USB commented part inside the bl_config.h file. Something is going wrong and we are not able to update the firmware either using UART or USB but as soon as I am commenting back those line my UART based boot-loader is working fine.
I am not able to find out the problem please let me know the possible reason for this. Prompt reply will be appreciated.
Thanks & Regards
Parvez Alam