Other Parts Discussed in Thread: DRV3205-Q1, DRV10987, DRV3245Q-Q1, DRV3245E-Q1
What are the applications in which these ICs are actually used?
It would be helpful if you could tell us a couple of types.
DRV10983-Q1
DRV3205-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the applications in which these ICs are actually used?
It would be helpful if you could tell us a couple of types.
DRV10983-Q1
DRV3205-Q1
Hello Akira-san,
DRV10983-Q1: This is a sensorless sinusoidal driver intended for automotive pumps and fans 2A RMS and below. This includes seat fans, motorcycle fuel pumps, and cooling fans. The DRV10987 is the industrial version of this part and is popular in pedestal/ceiling fans, air purifiers/humidifiers, dryer circulation fans, washing machine & dishwasher pumps, and medical blowers.
DRV3205-Q1 is intended for automotive functional safety systems such as EPS (electrical power steering), braking, and transmission. There is a newer family of automotive Functional Safety-Compliant drivers called DRV3245Q-Q1 and DRV3245E-Q1 which are recommended for these applications.
Thanks,
Matt
Matt-san,
Thank you for prompt reply .These are helpful.
Thanks
Akira