This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The inputs and outputs of 8343 don't match with the truth table. When output, the high-side MOS tube is always open, the low-side MOS tube cannot open. the output PWM of DSP TMS320F28035PNQ is in corresponding with the input of 8343.
Hi Zhao,
Is this the same question that Annie asked? LINK
Can you provide the SPI register settings that you are using?
Thanks,
Matt
Hi Zhao,
Thanks for the information. I'll get a response to you by the end of tomorrow
Best,
Johnny
Hi Zhao,
Thanks for the information. Try setting IC3-IC5 to 0x77 for to lower your IDRIVE to 65mA/130mA. As a note, also make sure that you are measuring GHx with respect to SHx and GLx with respect to SLx when measuring your gate outputs. Let me know if the problem persists.
Best,
Johnny