Hi,
I have two different motor driver. One is DRV8320S and the other is DRV8350H.
While I could control the engine very well with the DRV8320S, I couldn't do it with the DRV8350H. I also make the necessary resistance settings from the datasheet, but it did not work.
The settings I use in the DRV8320S are as follows.
spiSendData(DRIVER_CONTROL_ADDR, 0x3D0);
spiSendData(GATE_DRIVE_HS, 0x311);
spiSendData(GATE_DRIVE_LS, 0x711);
spiSendData(OCP_CONTROL, 0x059);
Could you tell me the closest resistor values corresponding to these settings? We have no idea what we did wrong.
Same card just changing Drivers.
Thanks,
Ali