This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8806: Solenoid driver recommend

Part Number: DRV8806
Other Parts Discussed in Thread: DRV8873,

Hi,

Customer search for solenoid drivers to apply to the rice cooker.

Please recommend a product that meets the conditions.

* Solenoid driver specification

Input voltage: 12V to 24V.

Driving current: 1.5 to 2A.

- Function.

PWM control according to feedback voltage.

Current limit can be adjusted by external resistance.

Input the driving current value to MCU.

  • Hello, Cho,

    "Input the driving current value to MCU." Is this a "must have" requirement? If yes, I would think DRV8873. The IPROPIx can be used to read the driving current by MCU. If not, DRV8806 looks good to me.

    Regards,

    Wang Li