I drove a brushless DC motor with a 20m DC cable and it stopped after a few seconds. However, if it is 17m, it will work without any problem. Please tell me why.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I drove a brushless DC motor with a 20m DC cable and it stopped after a few seconds. However, if it is 17m, it will work without any problem. Please tell me why.
Hi Nakamura-san,
Long cables add inductance to the supply. When motor is starting, spinning, or stopping, supply inductance can make it difficult to provide energy to the motor when it is changing current. Adding more bulk capacitance to the system should overcome supply inductance issues.
Thanks,
Aaron