Hi,
I have a previous design with SO-08 MOSFETs and want now to use D2PAK for better thermal resistance and also to have the decoupling caps near the FETs and still be able to use a coolant. Now I'm unsure about the placement of the MOSFETs and the path to the Gates are way larger than for SO-08 packages. Is there any problem in my placement of the motor driver and the MOSFETs? I think I minimized the parasitic inductances as way as possible, the only thing I could do is to have the DRV8350F on top of the FETs, but this will probably not really reduce the inductance, especially since vias are needed.
Kind Regards,
Sebastian