This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8818: IFS equation

Part Number: DRV8818

Hi,

In the datasheet, on page17, 8.2.2.2, IFS = VREF/(A*Risense) and in example, To achieve IFS = 1.25 A with RSENSE of 0.1 Ω, VREF should be 1.56 V.

Is this equation correct?

With 1.5V Vref, 0.2Ohm Risense, circuit is limited by 750mA.

Thanks.

  • David,

    The equation itself is correct, but the example is WRONG.  Example is section 7.3.2 is CORRECT.

    If you are using full step, this current will scale by 71% per table below copied from datasheet.

    Regards,

    Ryan