This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316REVM: 3x PWM Mode setup is descripted in an ambiguous way

Part Number: DRV8316REVM
Other Parts Discussed in Thread: DRV8316

Hello,

in ch 8.3.2.2 in the datasheet of DRV8316 rev.B you are describing the 3x PWM Mode and it's set up. The heading says " 3x PWM Mode (MODE = 10b or MODE Pin is Connected to AGND with RMODE) " but in figure 8-4 an resistor on MODE Pin is connected to AVDD.

Could please you clearify, which setting is correct? I know the "R" Version is configured in software, but in future design, we might want to have the possibility to use the non-spi version as an drop-in replacement.

Thanks,

Florian

  • Hi Florian, 

    Table 8-2 and the diagram is correct. The heading is incorrect and should be fixed to "3x PWM Mode (MODE = 10b or MODE Pin is Connected to AVDD with RMODE)".

    We will add this to our queue of datasheet errors. 

    Thanks,
    Aaron

  • Hi Aaron,

    thank you for your fast answer! You're talking about "queue" - sounds like more than one or two mistakes. Could you pass me a list with these errors or tell a date for the new revision of the datasheet? Would be amazing :)

    Thanks,

    Florian

  • Hi Florian, 

    We actually just released the production version of the DRV8316 datasheet last week, so this is actually the first item so far!

    Generally after a datasheet is released for production, we will internally document all datasheet errors that need to be fixed, and if there are enough significant errors to warrant a datasheet update, then we will do so. Since this just a typo as an error, this will not need an update yet. 

    Hope this helps, 
    Aaron