This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I'm designing a BLDC drive unit following the design material of the TI dev board DRV8328AEVM. I've already bought the gate driver DRV8328 and ideally I would have bought the same Mosfet devices of the TI dev board (CSD18536KTTT) but it's out of stock and unfortunately I couldn't find an available device from TI. However, I think I've found a suitable device from onsemi. The ratings are similar to the CSD18536KTTT but some parameters are different. For the CSD18536KTTT, the gate-source threshold voltage, gate charge and gate-drain charge are 2.2V, 108nC and 14nC respectively while for the onsemi device the values are 4V, 45nC and 7nC. So basically the device I'm choosing has got higher gate-source threshold voltage (4V instead of 2.2V) but lower gate charge (45nC instead of 108nC). Do you think it can still be controlled with the gate driver DRV8328? What external gate resistance value should I choose? I know that the selection of external gate resistance is an iterative process but based on the Mosfet and gate driver devices chosen is it possible to select a good staring value?
thanks
Giorgio
Hi Giorgio,
I think there might be a MOSFET gate-drive calculator tool somewhere on a product page, but will have to consult my team members for an answer on its location.
I think for an initial answer, below info should help:
MOSFET slew rate and turn-on profile:
internal resistances and source/sink current limits:
Slew rate control:
Best Regards,
Andrew
Hi Giorgio,
Just wanting to follow up here and see if my earlier answer helped resolve your question -
I followed up w/ a colleague and aligned that we don't currently have a calculator tool available for this, but will keep that in mind for future evaluations.
Best Regards,
Andrew
Hi Giorgio,
Just following up here - please let us know if my earlier answer resolved your question & mark the thread as such if that's the case.
Thanks!
Best Regards,
Andrew