The idea from the thread (DRV8662: Drives two cascaded piezo ceramic - Motor drivers forum - Motor drivers - TI E2E support forums) should be made a modification because the piezo is connected in a product in a way described in the following figure.
The following figure is the final design in the previous thread. Apparently, we should use two devices. Each device will output a 105V supply? How can they merged into a single supply?