Hi team,
Could u kindly help to check the following questions:
1.Is the spec IDRIVEP_HS the single bridge driven current? Is the value the peak value or valid value?
2. Could u provide the plot of IDRIVEP_HS over temperature?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could u kindly help to check the following questions:
1.Is the spec IDRIVEP_HS the single bridge driven current? Is the value the peak value or valid value?
2. Could u provide the plot of IDRIVEP_HS over temperature?
Hi Zoey,
1. The IDRIVEP_HS is the gate current used for switching on one of the high side MOSFETs. This is referring to the peak gate drive current.
2. We don't have a plot available of IDRIVEP_HS vs temperature, however I can say that at higher temperatures the IDRIVEP_HS gate current will trend lower and at lower temperatures the IDRIVEP_HS gate current will trend higher, all within the min/max rating of the IDRIVEP_HS spec for temperature between -40C and 150C
Regards,
Anthony Lodi