Part Number: DRV8910-Q1
Hello!
Is there a recommended order to send SPI configuration commands?
I want to get an application manual that describes the setting order.
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8910-Q1
Hello!
Is there a recommended order to send SPI configuration commands?
I want to get an application manual that describes the setting order.
Regards,
Hi,
Thank you for your questions.
-Datasheet has application and implementation section starting from page 129. It can be referred as user manual.
-No specific SPI command order requirements, however here is example.
1. Do not enable H-Bridge output (OP_CTRL_1 and OP_CTRL_2). Just leave them as default. - Please refer datasheet 8.3.1.1.4.6
2. Program other registers for configuration set up. (You may disable protections not used. e.g OLD_CTRL_1 and OLD_CTRL_2)
3. CLR_FLT in CONFIG_CTRL. This is optional but fault condition will be cleared.
4. Program H-Bridge output (OP_CTRL_1 and OP_CTRL_2) to start motor operation.
regards
Shinya Morita