Other Parts Discussed in Thread: MCT8316A, MCT8316Z
Hello, I am trying to spin up a small low power motor with the MCT8316AEVM. The motor does not seem to spin up with default settings on the board and the tuning does not seem to work to get a working setup. Please let me know if you can help me get this working for a motor with following parameters.
LOAD INERTIA ............................. 21 g.cm2
MAX SPEED ................................ 6000 RPM
DUTY CYCLE ............................... 100%
COIL INDUCTANCE .......................... 260 25% μH
COIL RESISTANCE ......................... 2.65 10% OHMS
Ke ....................................... 0.60 10% Vpk/KRPM
Kt ....................................... 0.81 10% N-M/ARMS
NUMBER OF POLES .......................... 12
Thank you,
Randy Holmberg