This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8910-Q1: Aging test before shipment

Part Number: DRV8910-Q1

Hello !

Customers requests critical circuits to be aging tested before shipment.

Are the following parts aging tested before shipment?

DRV8910

DRV8244

Please tell me about the contents of inspections that can be disclosed.

100% or sampling inspection

High temperature test (e.g. 125°C)

Low temperature test (e.g. -40°C)

Current value and ON time

Regards,