Other Parts Discussed in Thread: MCT8316Z, MCT8316A, MCF8316A, DRV8316, DRV8329, DRV8328, DRV8300, DRV8306, MCT8316Z-Q1
We are required to drive a 3 phase 24V, 3.1A BLDC motor. It is a sensored motor with hall effect sensors built in. It is our understanding you can simply use PWM connected directly to FETs to drive the BLDC motor. It is our understanding that you can use a basic gate driver to interface between the low voltage from the microcontroller to the higher voltage required by the FETs. It is also our understanding you can instead use a more sophisticated gate driver to simplify the control done by the microcontroller. Is this understanding correct? Can a meeting be set up to discuss the most suitable solution?