Other Parts Discussed in Thread: DRV8873, DRV8320
Customer asking if DRV8350 can operate with single H-bridge only. Can DRV8350 left two H-Bridge open and also work normally? thanks.
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Brian,
Yeah this can be done. I suggest Grounding INHx, INLX and SHx of the unused phases and leave the gates floating.
Best,
Akshay
Wouldn't the parallel connection of the two half bridges double the current capacity of the application? Even if the current is not needed, it would be a better use of the silicon inside the part, causing it to run a bit cooler. Just an idea...
Hey Lenio,
Based on Brian's phrasing I assumed he meant how to use only one half bridge since he said he wants to disable two h bridge.
Brian can you please confirm if you meant to disable two half bridges(two phases of the motor driver)?
Best,
Akshay
Akshay,
I did not mean to say the suggested solution wasn't valid; I just wanted to point out the paralleling of bridges as an alternative and as a way to better utilize the silicon in the device. I think Brian can play with both solutions and decide which one works best.
Cheers!
Hey Brian,
Please click the resolve button to let us know if this issue has been resolved.
Closing the thread for now. For further questions feel free to reopen the thread.
Best,
Akshay
Thanks.
in my customer application the DRV8873 is being used now for voice coil motor. However since the its package thermal issue, they are considering to use another solution.
DRV8320/50 is a common device for 3ph servo motor in that team, they are just wondering if two of half bridge of DRV8350 can be left disable and only uses one half-Bridge to drive DC motor
Hi Brian,
Is the customer trying to use the DRV8320/50 for a brushed motor application? If this is the case, they will need an H-bridge which would mean they would need to operate 2 of the half-bridges. Section five of the following FAQ (Quick Guide to Debugging Common Issues in BLDC motor drivers) which talks about this a little more.
Best,
~Alicia
Thanks Alicia,
Yes, it's a brushed motor application. and there are two H-Bridge needed. If DRV8350 is used, only one bridge needs to be disable.
Regards
Brian