This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8300: On the U/V/W three-phase, when the low-side MOS transistor is turned on, Vgs has a large return channel. Is it because the driving capacity is insufficient?

Part Number: DRV8300
Other Parts Discussed in Thread: CSD88539ND

Hi Team,

As shown in the figure below, csd88539nd is used for the MOS tube;

Schematic reference: DEMO_MD030A(001)_Sch;

The motor is a 13W BLDC motor, is this because of its insufficient drive capability? What improvement could I make?

This is the VGS waveform generated when the upper tube MOS is turned on. It has a long plateau period.

This is the VGS waveform generated when the lower tube MOS is turned on. It can only be opened with a large return channel.

Kind regards,

Katherine