Other Parts Discussed in Thread: DRV8316, TMS320F280025C, TMS320F280049C, C2000WARE, SFRA
Hey Team,
We have been working on developing motor controls and add features like FOC FW and MTPS using InstaSpin motion Library on LaunchXL - F280049C and DRV8316, but have been failing to find support or even proper documentation on how to develop source code for the same, For now we have been using this Universal Motor Control Project Manual and following the steps to use a custom board as we were not able to find any pre written example for DRV8316 with LaunchXL F280049c so we took a sample example for F280025c and then are trying to migrate it for F280049c. But there was no luck going ahead with that, that even created more build errors for us, We have made the following changes to the project configurations as well.
- Changed the Board and device type by double clicking on the .ccxml files in the project folder
- Renamed the .ccxml files to our processor from TMS320F280025C to TMS320F280049C
- Made changes to the pin configs according to pin mapping of f280049c
- We even changes the build configurations for the project
These are the errors that we encountered.
We think these errors are because the files in src_device are for f28002x but we need those for f28004x, can you aid us on how and where to get the device files for our specific controller.
Thanks
Shlok Desai