Other Parts Discussed in Thread: DRV8873, TMS320F280025, C2000WARE-MOTORCONTROL-SDK
Hello, this is the first time I am trying to design a motor controller to drive two Brushed DC motor, 5A Peak current each, with voltage, current, temperature and shoot-through protection, and dual-quadrature encoder for position feedback.
I need some assistance with selecting a general purpose Microcontroller that has UART interface and can perform control operation based on the position and error feedback. I am trying to determine between TI MSP430 and C2000 series. Appreciate your direction which controller would work sufficiently with DRV8873 integrated Driver (or other similar driver) that require minimum component count.
Is there any recommended reference design that use DRV8873 or similar?