Other Parts Discussed in Thread: DRV10987, DRV10975
Hi,
The customer uses the DRV10974 for the hot water mat motor control.
Stop after 1 to 2 seconds of motor initial operation.(current 0.9A)
Current Limit : 115kohm(1,400mA)
Motor phase resistance : 8.8ohm
BEMF : 2.9V(1500RPM)
However, it will work if the current limit resistor is modified to 12K or less.
Please review the schematic and give me advice on the problem.
Schematic : 7026.Schematic.pdf
Layout :
Normal waveform
Failed waveform