This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8251: Current Regulation bandwidth?

Part Number: DRV8251

Howdy,

I'd like to replace an analog closed-loop motor current driver with DRV8251 or similar.  Particularly interested in the internal current regulation, but require bandwidths in the 10s of kHz. Unfortunately, a couple of the scope traces in the datasheet seem to indicate pretty long settling times that would exclude this part (10s of ms).

Is there a simplified method to estimate current regulation bandwidth given some motor parameters, or is simulation the only way to go?  Alternatively, are there more suitable parts to explore (desire 3.5A+, 40V+ drive, full h bridge, internal current regulation, PWM drive).

Thanks!