This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV11873: DRV11873 device damaged

Part Number: DRV11873

hi,

DRV11873 drive motor does not rotate, please help analyze, thank you!

The test results are as follows:

a. Measure input voltage/signal is normal;

b. Measuring the motor drive board driver chip DRV11873, it was found that the motor drive chip is not working properly:

    1. Under normal input voltage of 12V, if the internal logic is not properly converted 5V voltage used;

    2. Measurement of impedance found that the impedance of the power pin of the motor drive chip is abnormally low 80ohm;

    3. Preliminary suspicion of damage to the internal LDO of the motor drive chip.

c. Cross validation:

    1. Cross the motor drive chip with a good motor drive board;

    2. Abnormal voltage and impedance follow the chip, and it is determined that the motor drive chip is damaged.

Schematic diagram: