Other Parts Discussed in Thread: USB2ANY
Hi Ti Expert,
We are using motor controller DRV10983Q1EVM and connected it with USB2ANY. The application is DRV10983Q1 EVM GUI.
We are operating a 3 phase BLDC motor. After giving 12V to motor controller for the 1st time, the motor started running.
The motor parameters given were :
i) Phase Resistance = 1.164
ii)BEMF Constant (Kt) = 73.6
The speed command range given in GUI is 0-511.
In our first attempt, we gave speed command of 511.
In this condition our motor achieved high speed and after 5 seconds the motor stopped.
Then we stopped the software and gave 100 value of speed command. But motor didn't work.
We restarted the GUI again and followed the same steps but motor didn't work.
Please help us regarding this concern and if there is any doubt, feel free to ask question.
Regards,
Vaibhav