Hi,
I have questions about retries in AlignMode.
Q1.
During an AlignMode operation, the ALIGN operation stops when the ALIGN_TIME has not been reached, and then ALIGN is performed again.
What are the causes of this retry?
Q2.
In some cases, the ALIGN retry continues several times, and the time from the start until the specified RPM is reached varies greatly.
The time to reach the specified rpm is usually 0.4s, but it can be as long as 2s, which may be a problem in terms of product specifications.
Please let us know if there is a setting to eliminate the retry factor.
We have prepared the attached documents to help you better understand Q1 and Q2.
Problem with multiple ALIGN in start-up.pdf
Thanks,
Conor