Other Parts Discussed in Thread: TPS8802,
Dear Team,
Do we have suitable solution can replace microchip RE46C100D8, thanks!
Condition
- PWM input 3.3V or 5V
- VDD 12-16VDC
- add 3pin (Buzzer)
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Thank you for reaching out. If the part is used for smoke detection or CO detection, the TPS8802 would be a good solution that could also replace other parts in the application. Another option if you just want a simple piezo driver would be the DRV2700, but you would have to use a buck converter as the input voltage is lower (VDD 3.3-5.5V) than your requirements.
Regards,
Sydney Northcutt