This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The DRV8889A-Q1 stepper motor driver is a variant of the DRV8889-Q1 driver with the following differences.
Programmable blanking time, tBLANK. As shown in the data sheet, section 7.3.7, the tBLANK can be programmed using the EN_SR_BLANK bit in the CTRL5 register.
Now you are all set to evaluate the DRV8889A-Q1 stepper motor driver using an DRV8889-Q1EVM.