This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8308: Is DRV8308 obsolete?

Part Number: DRV8308
Other Parts Discussed in Thread: MCT8329A

Hi Team,

The DRV8308 controller implements closed-loop speed control, allowing the motor to run at a precise speed over a wide load torque range.  It's required 100W of power to drive motors in customer's projects, so this device can meet the requirement. But the part number is currently not available on TI's official website under the Brushless DC Motor Drivers catalog. The customer would like to know if this device is still available or not? If not, are there alternatives? 

Could you help check this case out? Thanks.

Best Regards,

Cherry