This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8315A: BLDC QUESTIONS

Part Number: MCF8315A
Other Parts Discussed in Thread: MCT8316Z

Hi team,

I got several questions from customer. could you pls help to comment on it? Thanks!

1. How does the algorithm estimate the angle? What is the accuracy of the estimated angle? Does it affect the actual speed of the motor rotor? How much error is there?
2. Is angle estimation only supported by MCF8315? According to the MCF8315X device selection manual, if the peak winding current of the application does not exceed 5A, 
can it be understood that the performance of 8315 is better than that of 8316? 3. Is it possible to achieve extremely low speed control using sensorless FOC?

Rayna