Team,
Customer is working with TI’s DRV201 IC in a breadboard environment.
They can write to registers within this IC and confirm, via read back that the write occurred.
This is true for all but two of the registers.
In the DRV201 datasheet, registers 3 and 4 are used to determine the current drive from the part in the Register 7.6.1 address map
Is there something about those two registers that would cause them to be written to but the read back is not what was written?
Thanks in advance,
Aaron