This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8806: waveform issue

Part Number: DRV8806

Hi Team,

Use the DRV8806 to drive the stepper motor, please see the schematic and motor spec as follows:

By checking the waveforms for the four outputs A, -A, B, -B through the oscilloscope, it can be seen that there is a large overshoot voltage at the instant the coil is turned on, and there is also jitter in the working waveform:

The customer has also tried with the TBD62064APG from another corporation but cannot see the same issue, please see the TBD62064APG drive waveform:

Could you help check this case? Thanks.

Best Regards,

Cherry