This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3256-Q1: VGS_Lx_H Fault Not Clearing

Part Number: DRV3256-Q1

Hello,

We are getting a VGS_Lx_H on all phases over the SPI register. We noticed that clear faults helps us determine the active faults since a number of them latch while active. We measured the voltage at the gate and this is being driven to 12V from G to SL. All three phases report the same error despite that not being the case, which leads us to thinking t's latching. Is there a setting to clear this after reading other than sending the clear faults message?