Other Parts Discussed in Thread: DRV8251A
Hello,
We want to control a Linak LA14 motor using the DRV8701:
We want to control the motor in one direction: open or close. Could you comment on this if you see any challenges?
-This takes a couple of seconds. We do not want to PWM the drive signal.
-Control is done by a microcontroller
-Current is sensed by ADC of microcontroller.
-FET will be 2N7002K-T1-GE3 (3A) --> maximum current of Linak motor is 2A.
Could you comment on this if you see any challengs? Thanks in advance!