This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316AEVM: Bug / issue with EEPROM Controls in Motor Studio

Part Number: MCF8316AEVM

In Motor Studio, when one clicks under EEPROM Controls on "Read from EEPROM", the message that comes up is."This action will write all values to EEPROM registers".  It should say "read from" rather than "write to".  At least I hope so!  If it is in fact writing instead of reading, that's a giant bug.  If it's reading but has given the wrong message, it's very confusing.

Can you elaborate as to which action is being taken?

Please fix this error!

  • Hi Marc,

    This is indeed a typo in the pop-up dialog. However, the correct read/write actions are still performed accordingly despite the incorrect message when clicking on the Read from EEPROM button. This bug/typo has already been filed internally and has been addressed by our GUI developer for the next release.

    Regards,
    Eric C.