Hi support team.
My customer asked us regarding PWM_MODUL settings.
Q1:
The setting value 3h for PWM_MODUL is N/A.
However, it is configurable.
The motor is rotating.
Please tell us what this setting means and when to use it.
Q2:
When the speed command is low, it seems to be fixed at High side modulation.
PWM_MODUL settings are not reflected at low speeds.
Example: Set PWM_MODUL=2h(Mixed modulation)
-> When SPD_CMD=10%, it operates as High side modulation.
Is the above operation automatically performed inside the device?
Also, why is this behavior happening?
Best regards,
Higa