This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8315C-Q1: Compare with MCF8316C-Q1

Part Number: MCF8315C-Q1
Other Parts Discussed in Thread: MCF8316C-Q1, , MCF8315C

Dear, TI Support Team.

Is the difference between MCF8316C-Q1 and MCF8316C-Q1 only in the output peak current? If you have comparative materials, I would like to use them as promotional materials for customers.

MCF8315C-Q1 32Pin WQFN package and 24pin When will the HTSSOP product be released?

410h BUS_CURRENT Calculated DC Bus Current Register Regarding Section 6.8.5.3, there is a 32-bit value indicathing DC bus current iBus = (BUS_CURRENT / 2^27) * Base_Current / 8, but what is the definition of the calculation formula and what does Base_Current mean? I don't know if there are any. Is there any documentation on Base_Current?

Best Regards,
Hiroaki Yuyama