This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8306: Set the right R_ISEN value and power rating

Part Number: DRV8306


Hi,

In regard to the previous question, it was explain how to select the R_ISEN value (Based on the 0.25 Vlimit).

From that I derive that the power rating of the resistor should be I_max^2*R_ISEN.

If I look at the selected R_ISEN (CRE2512-FZ-R007E-3) from the DRV8306EVM (R29), it is a 7mOhm resistor of 3W of power.

I_limit will be about 35A (0.25/0.007) so P will be 35^2*0.007 = 9W.

In a stall situation or high load, the current can continue to be at the higher limit and the resistor will fail.

Am I missing something?

Thanks,

Tomer